Other Parts Discussed in Thread: UCC39002, TPS2411
Hi
We want to use LM74700-Q1 in an application where we have two redundant parallel power supply channels. Just like the application in the datasheet on page 21, Figure 36.
The supply will probably come from the same battery source with redundant cables supplying our unit, but it may also be from redundant battery sources in the future.
We would like to share the current evenly between both channels.
Can we expect the current to be shared between the both channels if we have the exact same input voltage at both channels?
If the voltage difference between the both channles then is greater then 11 mV, only one of the channels will be enabled, or?
I am affraid that we might be stuck in a state where only one channel at a time is enabled and that load transients will cause the voltage to drop a little bit and trigger a switch over to the disabled channel back and forth. And we will never benefit from current sharing between the channels.
What is your opinion about using LM74700-Q1 in this kind of current sharing setup?
Regards
/Johan