This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24298: Default state of PSEL and OTG

Part Number: BQ24298
Other Parts Discussed in Thread: BQSTUDIO

Can you verify that I am understanding the datasheet correctly?

If I hardwire the PSEL and OTG pins for a 100mA input current limit (PSEL - HIGH, OTG - LOW), I can raise that limit later using input current limit bits (IINLIM[2..0]) within the REG00 register?

When my board is initially powered on and prior to the USB port type being detected, I would like the bq24298 to default to a 100mA input current limit which is appropriate for a USB host port which has not been enumerated.  Once the type of USB port has been detected, I would like to update the input current limit (IINLIM[2..0]) and charge current (ICHG[5..0]) appropriately.  I plan to use the following settings based on the USB type detected.

USB Type IINLIM[2..0] ICHG[4..0]
USB 2.0 (SDP) 500mA (001b) 512mA (000000b)
USB BC 1.2 (DCP) 1.5A (101b) 1536mA (010000b)
USB Type-C 1.2 (DCP)

3.0A (111b)

3008mA (100111b)