Dear all,
Customer is looking for a DCDC solution with the below spec:
Vin: 45~60Vdc, Output: 12V/4A, Efficiency: >96%, Dimension: 20x40x10mm
Could you please help suggest any suitable solution? Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi:
can you whether LM76005 is fitting your application:
Datasheet Link:
EVM Link:
Hi Daniel,
Thank you. I am also checking this part. It seems that the only concern is the efficiency target. Do you have any idea on whether it can meet 96% efficiency?
Hi
you can use wenbench for efficiency estimation, I did it. for 48VIn 12Vo 200Khz 4A, efficiency around 96.3% in room temp.
alternative is controller soltuion(LM5145 or LM5146), You need use external fet, you can place the control part at bottom to minimize the soltuion space.
below is the LM5146 EVM test result with 12V output.
pls let me know whether it is helpful.