Other Parts Discussed in Thread: TLV62130
We use TPS54627 circuit,whistling when using dynamic load. it"s normal when useing static load .we check the Spec,No abnormal problems found。 could you explain why?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, What's you dynamic loading frequency?
Yuchang
I try the frequency from 1K、6K、10K using electronic load, I hear the different whistling.
Seems It should be related to the loading transient frequency, which is in audio frequency area 20-20kHz.
Did you confirm the whistling was from inductor or the output caps?
Please upload you schematic for review.
Yuchang
Sch as attachment.
I'm not sure the whistling is from inductor or outpue cap. It seems the whisting is from IC.
I try the tantalum capacitors and Electrolytic caps as output caps , whistling is a little smaller than before.but I can hear it.
And we also change the inductor to 3.3uH and 4.7uH, the same phenomenon.
We try the IC TLV62130, the samen dynamic loader,Also has the whistling. we try the TI TLV62130-EVM board,the same whistling
It strongly related to the loading transient frequency
Yes, it is related with loading frequency as I said.
Based on you test result, I suppose the whistling comes from input MLCC, IC does not generate the audio noise, you can change input caps to pos-cap or tan-cap to check.
Yuchang
Change C1366 to 1uF, and recommend to change C1367 to 22uF for backup based on testing result to determine stuff it or not. others looks well.