Hi,
When building bus powered devices with analog/audio functionallity, usually you need to rely on a stable 5.0V for an ADC.
As USB bus power can be anything between 4.4V to 5.1V depending on cable length, hubs in series, etc, I'd like some guidance finding an optimal dc/dc to boost vbus to 5.0V.
It's a bonus if there is some sort of 100% on/pass-through mode if the rail is already above the set output voltage (for best efficiency)
I expect current draw to be as little as <= 20-30mA at most.
Thanks
David