Tool/software: WEBENCH® Design Tools
Hello! I have a question on TPS5430. The are a lot of scheem design in datasheet, I don`t know which reference design I should take. Which difference between scheem on page 13 and 23?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
Hello! I have a question on TPS5430. The are a lot of scheem design in datasheet, I don`t know which reference design I should take. Which difference between scheem on page 13 and 23?
Hi,
I think both schematic are similar. The things that i see a difference is the inductor selection between 15uH and 22uH and i believe that could relate to the input range difference between 2 design.
Therefore you can select either design based on your specification.
Alternatively, you can also follow the EVM design that has sample result
https://www.ti.com/lit/ug/slvu157/slvu157.pdf
Thanks
-Arief
Hi! Anyway, is ceramic output filter used for which reason? Which advantages by comparing with circuit on electrolytic capasitor?
Electrolytic capacitor with sometimes, large finite ESR will result in additional output ripple.
In addition, ESR will need to be consider and extra considerations may be requiring in doing loop analysis.