This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27441-G1: Connection of BQ27441 fuel gauge sensor along with the BQ24075 LiPo Charger

Part Number: BQ27441-G1
Other Parts Discussed in Thread: BQ24075, BQ27411-G1

Dear TI-Team,

I would like to use a BQ27441 fuel gauge sensor for a LiPo battery and a BQ24075 for charging.

I am wondering where to connect the SRN-Pin of the BQ27441. In the datasheet, it reads, the pin should be connected to VSYS. Intuitively, I would put it to my 3.3V VCC rail.

Also, could you please have a quick check if the connections from the LiPo battery to the fuel gauge and the charger circuit are correct?

I've inserted screenshots of the components at the end of this thread.

Thank you for your help!