This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28051: Can i use UCC28051 for PFC fly-back converter?

Part Number: UCC28051
Other Parts Discussed in Thread: PMP11155, UCC28050

Hello, I am planing to use UCC28051 for fly-back converter with optocoupler  feedback compensation. PFC and THD  are the major parameters that i have to achieve.

Please suggest shall i go ahead or any other part no. you can suggest me.

Output Power : 40W

Output Voltage : 24V

  • Sudhakar

    Yes you can.  UCC28050 (which is the same as UCC28051 except UVLO threshold and gM amplifier values are slightly different, and they share the same datasheet) can be configured as such.  PMP11155 is an example of UCC28050 configured as a PFC flyback with optocupler feedback.

    Best Regards,

    Eric