This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS77001 as battery charger : Is there an alternative part with load disconnect??

Other Parts Discussed in Thread: TPS731

Hi all!

Below you can find my schematic for using the TPS77001 as a battery charger.

Its input is a voltage supply of around 5V or less, which is not always present and which can supply a maximum current of around 25mA. The output of the regulator is adjusted at 3.7V and the battery is connected directly to its output. The Enable control input is driven by a microcontroller. As you can see, I haven't used any diode between the regulator and the battery, in order to avoid its voltage drop. However, it has been proved that this point is a little bit problematic. Although I keep the EN input to LOW, when the voltage supply is not present, I have noticed that the voltage at the input of the regulator is around 2.7V, when the battery voltage is around 3.3V Since there is no other voltage source present (as I said, the voltage supply which charges the battery is not active during this phase of the test), I guess that there is some leakage from the battery through the VOUT pin of the TPS77001 going out from the VIN pin.

Can you verify, please, that this is possible? I guess that there is no real disconnection of the load during the period when the regulator is not enabled, is that true? Is this the reason that I see this problem?

In that case, I guess I should use some kind of switch between the regulator and the battery, which will be activated only during charging. Another alternative I was thinking is using another LDO instead of TPS77001 that can provide real load disconnect during shutdown. Is there such a part? Ideally, I would prefer to be pin to pin compatible with TPS77001, but I guess this would be really difficult. Nevertheless, any substitution with this load-disconnect feature would make me happy as well!

Thank  you very much in advance!

Nikos

  • Most linear regulators with FET pass elements have the FET's body diode that allows current flow from Vout to Vin, even if not show in the datasheet's block diagram. 

    The TPS73x01 family of regulators has reverse leakage protection but its pin out is different than that of the TPS77001.

    You might also consider one of our bq24xxx or bq25xxx linear battery chargers.  They offer more features than a simple linear regulator.

  • Thanks for your quick reply Jeff.

    I have read the datasheet of the TPS73001, but unfortunately I haven't found anywhere that it has reverse leakage protection. Actually it is stated in the datasheet (under the "Regulator Protection" section) that the regulator allows current to flow from the output to the input during shutdown, which is exactly what I see with the TPS77001, too. Anyway, thank you a lot for your help. Regarding the bq24xxx and bq25xxx, I have indeed considered using one of them, but the problem is their large current consumption when charging the battery.

     

    Nikos

  • Hi again Jeff!

    After doing some search, I have found the TPS73201 part. This indeed has reverse current protection, isn't that correct? Moreover it is pin compatible with TPS77001. The only drawback I can see is that its GND pin current is quite large (~0.5mA), but I guess it is the only alternative I have for the time being.

    Nikos

  • Yes, the TPS730xx is a different IC than the TPS731/2/6xx.  I apologize for the confusion.