This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27441-G1: Erroneous Full Charge Capacity

Part Number: BQ27441-G1

Hi all,

I would like to use a battery that I can disconnect and reconnect. For this purpose, I followed the BQ27441-G1 Quickstart guide and save the Ra Profile and QMax Cell 0 in the processor non volatile memory as preconised.

On POR detection, the Ra Profile (Ra0_0 to Ra0_14) and QMax Cell 0 are written back to the gauge flash. The Config Update Mode is exited using the ExitResim command.

The gauge default design capacity is 1340mAh, my battery is a 2000 mAh (by the way, the Design Capacity, Design Energy, Taper Rate, and Taper Voltage, are correctly set in the gauge flash data).

When I fully charge the battery, the estimated full charge capacity is around 2080mAh. If I unplug the battery and plug it again (flash restored), I expected to have a full charge capacity around the previous value but instead I get around 1280mAh.

What did I miss?

Thanks,

Alex