I'm using a TPS62823 in a 5V to 3.3 V step down application. In our application the power input input cable is very long and when plugged in we see an 8V transient as measured at the input capacitor:
Obviously this exceeds the recommended 6V max input for the TPS62823. I'd like to replace the input ceramic with something with a higher ESR like a tantalum or electrolytic to avoid this overshoot, but I do not see minimum ESR guidelines in the datasheet and webbench simulations with varied ESR on the input capacitor don't seem to effect stability which makes me think either something is wrong in the simulation or the datasheet guidance is incomplete.
so I have two questions 1. is an input transient of that magnitude acceptable? and if it's not what's an acceptable value for input capacitor ESR