This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25145: LM25145

Expert 1215 points
Part Number: LM25145

Hello,

I'd like to ask to what extend can I increase inductor ripple current using LM25145?

Could it be up to 100%? 150%?

I'm asking only about stability issues - whether this regulator can work in high DCM mode, switch between CCM, DCM whil load is changing?

Because this is voltage-mode controled chip, right?

Not asking in terms of Out Cap ESR or Inductor power.

Regards, 

Adam