Other Parts Discussed in Thread: LM5141, LM61460, TPS40170
Hi,
I have a question about DC DC Converter. The question is that, in light load, the converter quescient current is 25mA. But I want to decrease this current in no load conditon. To 1mA. Our controller tps40170-Q1. The OEM's spec is that the quesient current must be lower than 5mA. How can I solve this problem? Is there any chip to control the Enable pin ?