This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL2575HV-12: Absolute Max Supply voltage the same as Max Recommended Operating Supply voltage

Part Number: TL2575HV-12
Other Parts Discussed in Thread: LM5164

I'm looking to include the TL2575HV-12 regulator within a design of mine to provide bias to a larger power converter. This the main power converter will function within a supply range of 40-60V, potentially up to 65 V for short periods of time (Over-voltage protection limit).

The datasheet for the TL2575HV-12 lists the max recommended operating supply voltage as 60V, I was therefore surprised to see the absolute max supply voltage also listed as 60V. Is this product safe to use at 60V? or is the absolute max voltage listed incorrectly?