I'm trying to make my own charger for a Li-ion battery pack, and I'm having a problem with the NTC Fault showing Warm in Battery Management Studio when a USB 5V supply is applied. I intend to use a battery fuel gauge along with the bq25895M, so I just have 2 10K resistors creating a divider between REGN - TS - GND. I measure 2.5V at the TS input and 5V at REGN, but the chip seems to think the NTC is warm, and I suspect that is the reason it does not charge. What to do?