This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG3410R050: 900-V GaN solution for grid and beyond

Part Number: LMG3410R050


Key highlights and features:

  • 5kW bidirectional AC/DC grid converter using GaN
  • Achieves 99% efficiency, with no forced air cooling
  • Supports bus voltages up to 1400V
  • Features LMG3410R050: 600V 50mΩ GaN with integrated driver and overcurrent protection, and C2000 digital controller

For more details about this demo, please visit 

https://training.ti.com/900v-gan-solution-grid-and-beyond

Please follow up on this post for any questions related to this design!