This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS780: input cap

Part Number: TPS780


Hello,

I had a question on the TPS780230300DRV. I was looking through the datasheet and saw the recommendation about the input capacitance. Due to other functions on the same input line, I am looking to increase the capacitor to either 2.2uF, 4.7uF or 10uF. They are all going to be X5R or X7R. Could there be any potential concern with using a higher value input capacitor than the recommended value of 1uF from the d/s?

Thanks for the helP!

Best,

Adam

  • Hi Adam,

    The input capacitor for an LDO is not required for stability. This is simply to minimize voltage droop due to inrush or a sudden load surge.  You can make this as large as you like.

    Regards,