This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55340: no starting

Part Number: TPS55340


I am pasting this schematic for I need help into turning the Boost die on. I have all voltages at:

VIN=15V

Vout=14.8V

SS=2V

Comp=0.7V

FB=1.64V

EN=5V

SW=15V

No switching at all

boost.pptx