I'm looking to use the LM74670-Q1 in a very low current use case (300 nA - 1 mA).
The problem is that the intrinsic body diode in MOSFETs doesn't generate the minimum 0.48V forward voltage that the LM74670-Q1 requires when currents are that low (or just barely at 25C, but not when it gets warmer).
Is there a solution for low current cases such as mine?  
For example, can the LM74670-Q1 work with IGBTs?  Since IGBTs don't have intrinsic body diodes, it might be possible to add a discrete diode with more suitable properties.  And/or is there a better option?  
Thank you.