This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23758: Whether there is an IC that meets the requirements of the following parameters, the whole scheme can be recommended.thank you

Part Number: TPS23758
Other Parts Discussed in Thread: BOOST-PSEMTHR-007, TPS23881EVM-008, TPS23881

Hi Friend;

    Whether there is an IC that meets the requirements of the following parameters, the whole scheme can be recommended.thank you
 
60W 5 Gigabit POE Power supply
1.Input Range;100-240Vac,50/60Hz
2.Output;48VDC 1.25A 60Watt
3.Desk-top type with IEC320-C14,3 pins socket
4.Support 10/100/1000/5000Mbps Gigabit
5.Pin 4536+/127878-,4 pairs
6.UL Certified

  • Hi Tony, 

    Thank you for your question. Unfortunately we do not have a reference design that meets the criteria you have provided.

    For 60W, 4-Pair power levels I recommend designing with the TPS23881 PoE PSE IC. We have a very easy to use evaluation module which consists of the TPS23881EVM-008 daughter card and BOOST-PSEMTHR-007 mother board that I recommend ordering which can be used to evaluate this PSE IC for use in your system. 

    Please let me know if you have any additional questions and thank you for your interest in Texas Instruments PoE devices. 

    Best Regards, 

    Brett Colteaux

    PoE Product Marketing Engineer

  • Hi  Brett Colteaux

             Thank you