This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: LiFePo accuracy

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQ34110

Hi,

using the BQ34z100-G1, I see huge jumps on SoC, after a charge cycle (from 25% to 60%, unplugg, let it rest for 12h, then it shows like 92% SoC).

I also discovered that during charging, the BQ returns 0V.

Any idea?

Thanks

Christian