This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5113-Q1: Is it not suitable for using GaN with source to drain current flowing?

Part Number: LM5113-Q1
Other Parts Discussed in Thread: LM5113

Hi team, 

Should GaN use only for drain to source current flowing? Is GaN not suitable for replacing FET in phase shifted full bridge rectifier? 

I saw document which descrives GaN. They said that "GaN's third quadrant" leads high drain to source voltage. 
I understood that it is not suitable for using GaN in third quadrant condition and it should be use only for drain to source current flowing condition such as bridgeless totem pole PFC. Is this understanding correct or not?

Regards,
Ochi