Hi,
I have an application with a high capacitive load of 2000uF sitting on a plugable board. Main reason for the 2000uF is that the board can be unblugged and the power need's to stay up and running so that the supply can run a controlled power down sequence.
The issues is that when the board is plugged in, the TPS22920 will, when the baord is detected, switch on and charge the cap, but based on the guidllines from the Datasheet the inrush current should not exceed 40mA is this a correct reading? Since the switch can handle 4A RMS and 6A peak, I wonder why there is a limit of 40mA?
What is from Design point o view the max. ammount of capacitance which could be used with the TPS22920 when using a 3.3V supply?
If using a supply (Vin) which is always on and can support a fast transient response , would you still request Cin 10x Cout ?
If you think the TPS22920 is the wrong device for this kind of application, what would be your advice , should we use mor a eFuse or a hto swap device since you can limit the current easier ? Any advice suggestion is OK
Looking forward to your feedback.