1.Can The reference design use USB Interface Adapter Evaluation to connect?
2.Why did it used V2 as temperature sensor positive?
As datasheet reference ,"VLDO2 respect with V2 3.0v".
A Li-ion Cell voltage is 3.6V.
It means VLDO2 is 3.6+3.0V.In my opinion,temperature used 3.6V was enough.
Why should it be 3.6+3.0.
Is it correct?
Thanks for your faovrs.