This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24735: Simultaneous 6 A SYS Output and 3 A Single-Cell Li-Ion Charging

Part Number: BQ24735
Other Parts Discussed in Thread: BQ28Z610-R1, BQ24773, BQ24610

Hello,

I'm looking for some suggestions on a power management design.

I would like to use a fuel/gas gauge IC (BQ28Z610-R1) combined with a compatible I2C-controlled battery charger capable of supplying 6 A "system" output while simultaneously charging a single-cell Li-Ion battery at 3 A.

Input can be either 5 V USB or < 15 V wall adapter.

Are you able to recommend any battery chargers that meet these specifications or are these current requirements too high?

Thanks,

Kevin