This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25619: How to set RT1 and RT2, so that the IC in the temperature range of 15~45℃ normal charging, not in this range on the suspension of charging?Is there a calculation table for BQ25619 TS NTC?

Expert 2630 points
Part Number: BQ25619

How to set RT1 and RT2, so that the IC in the temperature range of 15~45℃ normal charging, not in this range on the suspension of charging?Is there a calculation table for BQ25619 TS NTC?


R25          10      k ohm +/-       1           %
  B(25/50)      3380       K +/-         1           %
   TEMP.       R-low      R-center     R-high
  (deg.C)     (k ohm)     (k ohm)     (k ohm)
    -40       188.0202    195.6520    203.5731
    -39       177.8044    184.9171    192.2951
    -38       168.2141    174.8452    181.7195
    -37       159.2069    165.3910    171.7981
    -36       150.7435    156.5125    162.4860
    -35       142.7877    148.1710    153.7418
    -34       135.3055    140.3304    145.5274
    -33       128.2659    132.9576    137.8071
    -32       121.6397    126.0215    130.5481
    -31       115.4001    119.4936    123.7198
    -30       109.5221    113.3471    117.2940
    -29       103.9894    107.5649    111.2522
    -28       98.7725     102.1155    105.5611
    -27       93.8512     96.9776     100.1981
    -26       89.2071     92.1315     95.1423
    -25       84.8227     87.5588     90.3741
    -24       80.6819     83.2424     85.8755
    -23       76.7698     79.1663     81.6295
    -22       73.0722     75.3157     77.6204
    -21       69.5761     71.6768     73.8336
    -20       66.2694     68.2367     70.2554
    -19       63.1477     64.9907     66.8807
    -18       60.1923     61.9190     63.6889
    -17       57.3933     59.0113     60.6689
    -16       54.7415     56.2579     57.8105
    -15       52.2283     53.6496     55.1040
    -14       49.8456     51.1779     52.5406
    -13       47.5859     48.8349     50.1117
    -12       45.4422     46.6132     47.8097
    -11       43.4078     44.5058     45.6271
    -10       41.4765     42.5062     43.5570
     -9       39.6345     40.5997     41.5843
     -8       37.8855     38.7905     39.7131
     -7       36.2244     37.0729     37.9374
     -6       34.6461     35.4417     36.2519
     -5       33.1462     33.8922     34.6515
     -4       31.7202     32.4197     33.1313
     -3       30.3641     31.0200     31.6869
     -2       29.0740     29.6890     30.3140
     -1       27.8465     28.4231     29.0088
     0        26.6780     27.2186     27.7675
     1        25.5690     26.0760     26.5904
     2        24.5123     24.9877     25.4698
     3        23.5052     23.9509     24.4026
     4        22.5450     22.9629     23.3861
     5        21.6294     22.0211     22.4175
     6        20.7560     21.1230     21.4944
     7        19.9227     20.2666     20.6143
     8        19.1273     19.4495     19.7751
     9        18.3680     18.6698     18.9745
     10       17.6430     17.9255     18.2107
     11       16.9494     17.2139     17.4807
     12       16.2870     16.5344     16.7840
     13       15.6541     15.8856     16.1189
     14       15.0493     15.2658     15.4838
     15       14.4712     14.6735     14.8772
     16       13.9184     14.1075     14.2977
     17       13.3898     13.5664     13.7439
     18       12.8841     13.0489     13.2145
     19       12.4002     12.5540     12.7084
     20       11.9371     12.0805     12.2244
     21       11.4945     11.6281     11.7621
     22       11.0703     11.1947     11.3195
     23       10.6637     10.7795     10.8955
     24       10.2738     10.3815     10.4892
     25        9.9000     10.0000     10.1000
     26        9.5343      9.6342      9.7342
     27        9.1838      9.2835      9.3833
     28        8.8477      8.9470      9.0465
     29        8.5254      8.6242      8.7234
     30        8.2162      8.3145      8.4132
     31        7.9204      8.0181      8.1162
     32        7.6367      7.7337      7.8312
     33        7.3647      7.4609      7.5576
     34        7.1038      7.1991      7.2951
     35        6.8534      6.9479      7.0430
     36        6.6131      6.7067      6.8009
     37        6.3825      6.4751      6.5683
     38        6.1611      6.2526      6.3449
     39        5.9485      6.0390      6.1302
     40        5.7443      5.8336      5.9238
     41        5.5474      5.6357      5.7248
     42        5.3582      5.4454      5.5333
     43        5.1764      5.2623      5.3492
     44        5.0015      5.0863      5.1720
     45        4.8333      4.9169      5.0015
     46        4.6715      4.7539      4.8373
     47        4.5159      4.5971      4.6793
     48        4.3661      4.4461      4.5271
     49        4.2220      4.3008      4.3806
     50        4.0833      4.1609      4.2395
     51        3.9498      4.0262      4.1036
     52        3.8213      3.8964      3.9727
     53        3.6975      3.7714      3.8465
     54        3.5783      3.6510      3.7249
     55        3.4634      3.5350      3.6076
     56        3.3527      3.4231      3.4946
     57        3.2461      3.3152      3.3856
     58        3.1432      3.2113      3.2804
     59        3.0441      3.1110      3.1790
     60        2.9486      3.0143      3.0812
     61        2.8578      2.9224      2.9881
     62        2.7703      2.8337      2.8984
     63        2.6858      2.7482      2.8118
     64        2.6044      2.6657      2.7282
     65        2.5259      2.5861      2.6476
     66        2.4501      2.5093      2.5697
     67        2.3770      2.4351      2.4945
     68        2.3064      2.3635      2.4218
     69        2.2382      2.2943      2.3517
     70        2.1724      2.2275      2.2839
     71        2.1086      2.1627      2.2181
     72        2.0469      2.1001      2.1545
     73        1.9873      2.0396      2.0930
     74        1.9298      1.9811      2.0335
     75        1.8741      1.9245      1.9761
     76        1.8204      1.8698      1.9205
     77        1.7684      1.8170      1.8667
     78        1.7181      1.7658      1.8147
     79        1.6695      1.7164      1.7644
     80        1.6225      1.6685      1.7157
     81        1.5772      1.6224      1.6687
     82        1.5334      1.5777      1.6232
     83        1.4909      1.5345      1.5792
     84        1.4499      1.4927      1.5365
     85        1.4101      1.4521      1.4952
     86        1.3717      1.4129      1.4552
     87        1.3344      1.3749      1.4165
     88        1.2984      1.3381      1.3790
     89        1.2635      1.3025      1.3426
     90        1.2296      1.2680      1.3074
     91        1.1966      1.2343      1.2730
     92        1.1647      1.2016      1.2396
     93        1.1337      1.1700      1.2073
     94        1.1037      1.1393      1.1760
     95        1.0746      1.1096      1.1456
     96        1.0464      1.0807      1.1161
     97        1.0190      1.0528      1.0875
     98        0.9925      1.0256      1.0598
     99        0.9668      0.9993      1.0328
    100        0.9419      0.9738      1.0067
    101        0.9179      0.9492      0.9816
    102        0.8946      0.9254      0.9571
    103        0.8720      0.9022      0.9334
    104        0.8501      0.8798      0.9104
    105        0.8288      0.8580      0.8881
    106        0.8081      0.8368      0.8664
    107        0.7881      0.8162      0.8453
    108        0.7686      0.7963      0.8248
    109        0.7497      0.7769      0.8049
    110        0.7313      0.7580      0.7856
    111        0.7135      0.7397      0.7668
    112        0.6962      0.7219      0.7485
    113        0.6793      0.7046      0.7308
    114        0.6630      0.6878      0.7135
    115        0.6471      0.6715      0.6968
    116        0.6316      0.6556      0.6805
    117        0.6166      0.6402      0.6646
    118        0.6020      0.6252      0.6492
    119        0.5878      0.6106      0.6342
    120        0.5740      0.5964      0.6196
    121        0.5606      0.5826      0.6054
    122        0.5476      0.5692      0.5916
    123        0.5349      0.5562      0.5782
    124        0.5226      0.5435      0.5651
    125        0.5106      0.5311      0.5524

 

  • Hi,

       This part employs JEITA according to industry standard JEITA guideline. Sizing the RT1 and RT2 resistors give you control over what temperature the T1 and T5 thresholds correspond to. In the datasheet, the example they take is to set T1 = 0C and T5 = 60C. You can adjust RT1 and RT2 according to your expected T1 and T5 thresholds (based off of the thermistor you have chosen), and then calculate what T2 T3 T4 thresholds will be.