I'm using a pair of TPS54531 devices to generate 5V and 3.3V from a 24V source. I have been going through the datasheet figuring out the components to meet our power requirements. And then I ran into section 9.2.2.6 Compensation Components. To calculate the values of these components you need to run a Spice simulation and generate two values to use in Equation 17. (Actually I'm not sure by description what those values are.) I don't have access to a spice tool nor do I know how to use one. I've downloaded and installed TI's Tina tool but I don't know how to use it. Supposedly Webbench will help but I can't seem to find my way to it. Is there another way to determine the values of these components?