This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV759P: FB constant setting

Part Number: TLV759P

Hi,

I asked a question in the following thread about setting the device constant of TLV759 before.
With that advice in mind, I came up with the following constants:
Is it OK to use this constant?

VOUT: 4.9V
R1 = 174kΩ, R2 = 22kΩ, Cff = 0.1uF
VOUT: 4.3V
R1 = 150kΩ, R2 = 22kΩ, Cff = 0.1uF

Best regards,

e2e.ti.com/.../3288556