This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC28025: UC28025D - Whether suitable for interleaved dual forward design

Part Number: UC28025
Other Parts Discussed in Thread: UCC28220

Does this IC suitable for interleaved dual forward design?

If yes, any app note or ref design?

BR,

Gary

  • Hi Gary,

    The UC28025 is not suitable for interleaved dual forward designs.

    It was designed for double ended applications such as full and half bridges as well as push pull .

    The UCC28220 is a dual interleaved controlled suitable for interleaved forward applications.

    Regards

    John