Part Number: UCC256404
Other Parts Discussed in Thread: UCC256402
Hi,
I wanted to know whether UCC256404 can support the AC input for it's HV pin with a frequency range of 380 to 800 Hz or not ?
Regards,
Vineet
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Vineet,
The HV startup function will work just fine at higher AC frequency. The X cap discharge function will work as well but I would be curious what X cap discharge standard do you need to meet. Is this for an avionics application? We currently have CB certificates for IEC60065, IEC60950 and IEC62368. Do you know which X cap discharge standard you need to satisfy for your design?
If X cap discharge is not needed, you could use UCC256402 which has high voltage startup with no X cap discharge function. With UCC256402, you can connect the HV pin to either AC or DC input.
Best Regards,
Ben Lough