This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5575: output inductor selection

Part Number: LM5575


Hello,

Due to non-availability of high (68uH or 47uH) value with high current inductors in our database, we are planning to reduce the inductor value to 33uH by increasing the Ip-p. to 1.2A

 

As per the calculation, only output capacitor value I have to increase.

 

My question is:

  

is there any impact on the efficiency or any other functions?

 

I have consider below.

 

Vout : 15V

Output Ripple : 100mV

Iout : 0.6A

Fsw : 260Khz

 

Kindly clarify.