Other Parts Discussed in Thread: UC2843
Tool/software: WEBENCH® Design Tools
Hello,
I am not able to understand the function of auxiliary winding of the flyback transformer connected to the Vcc pin of the switcher. Input DC voltage is also connected to the Vcc pin via startup resistor network. What is the role of Raux ,Daux and Cvcc and how is the turns ratio of Auxiliary winding achieved? Please explain in detail
Input voltage range is 10 - 26 V DC from a battery
Thanks and Regards