Other Parts Discussed in Thread: LM5060, , LM5069
I'm designing the 74700-Q1 into the front-end of an on-board mobile dc-dc converter/battery charger. The design will operate in both 12V and 24V systems to charge a 12V AGM battery. The applications note on page 18 of the 74700 spec recommends back-to-back TVS diodes of 58V to the high-side and 26V to the low side, based on the ISO spec. These are working voltage ratings, not breakdown voltages. The SMBJ58A Vbr is: 64.4Vmin, 71.2Vmax.
My question is this: Given the max input voltage of the charge controller I'm using is +/- 60V, could you offer any thoughts/suggestions on meeting the ISO spec while not violating the 60V spec for the rest of the design? Am I missing something? Charge controller is LTC4020.
Thx,