Looking at the maximum rating for CSD95490Q5MC at VOS, its specified a max of 7V, from Pgnd to the VOS pin.
If the IC was to be used in buck mode, does it mean the max output will have to be well under 7V ?
Most of the development examples I see using this IC are making 0.8V, 1V and 1.2V outputs.
Please clarify what would be maximum recommended output for this IC.
Thank you