Other Parts Discussed in Thread: BQ25606, BQ27426
I would like to us BQ27421-G1 together with the battery charger BQ25606.
I have two questions:
1. Would using the BQ27421-G1 negatively affect the charging in any way?
2. Would it be correct to connect the SRX pin of BQ27421-G1 to the BAT pin of BQ25606?
3. Our device draws up to 4A (continuous) from the battery. Will the BQ27421-G1 provide accurate readings?
Thank you in advance.