This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD19535KTT: VDS leakage current increase over time

Part Number: CSD19535KTT


hi Team,

it's reported by our customer on one of the CSD19535KTT IC

it's observed that the VDS leakage current will increase over time, can we have your comment on this?

VGS:200kohm

VDS: 28.8V

monitor VDS current:

the test is done in room temp, after two hours the VDS leakage current seems to increase

although it's still within spec, but this behavior does not happen on other batchs of CSD19535KTT IC

may we check with your comment on this? whether need to have FA analysis?

standalone MOS leakage test under room temp, here is the Vds leakage measurement