This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40200: With the P-FET for small parasitic capacitance

Guru 11170 points
Part Number: TPS40200

Hello E2E,

When with small the parasitic capacitance of P-FET, VGDRV goes to under 10-V from VDD at FET turn-ON.

Questions;
What Is cause?
Is there any countermeasures?
Vin 24V - 36V, Vout 12V, Iout 1A, What is the recommended P-FET?

Regards,
ACGUY