Other Parts Discussed in Thread: BQ7718, BQ77915, BQ78350
Hi,
I have one consult for BQ77905. Customer has used BQ7718 with only OV protection. Now, they want to implement OV/UV protection together and I have promoted BQ77905. However, here is some consult from Positec.
a. Customer only want UV/OV indication signal without external MOS and do not need OCP, OT, UT and OW now. Can they only use DSG/CHG for indication?
b. BQ77905 should support hot plug, ex, when plugging first cell first or third cell first, BQ77905 is not broken.
c. OV indication signal(CHG) should be safely turned on when BQ77905 fail. As in UL2595 standard, battery should not be over-charged in case any of device fails.
.