This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5060: Circuit simplify to the example design in datasheet

Part Number: LM5060
Other Parts Discussed in Thread: LM76202-Q1, , TPS2660

Hi team,

We want to use LM5060 to make the function of avoiding user connecting VIN and GND in contrast.

However, there are too many components in the example(more complex than our original discrete solution).

Original design only use 2 back to back MOSFET, 1 BJT, 2 diodes, and some resistors.

May I know that which components can be omitted?

And could it make to do OCP at 2A current?

The end equipment is professional audio mixer/control surface.

Thank you.

Best Regards,

Cindy