Other Parts Discussed in Thread: BQSTUDIO
In BQ27441-G1, the GPOUT pin#12 is multiplexed, I’ve two questions,
By default OpConfig [BATLOWEN] is cleared, How to set it? If it is set, it will act as a BAT LOW Indicator.
If StateOfCharge() < SOC1 Set Threshold, the [SOC1] flag is set, means the GPOUT pin will drived to LOW. The default SOC1 Set Threshold = 10%. How can I change the SOC1 Set Threshold Value?
And once I set it, will it be stored in it’s memory?