Hello team,
I'm trying to fully understand the working principle of BQ77915 and I have a question regarding the OV limits.
1: So if 4.2V/cell is a standart voltage for Li-Ion batteries and my charger is set to 4.2V and the OV of BQ77915 is also 4.2V it means that it won't charge the battery since it will enter in OV state? Or are the 7791500 and 7791502 designed to protect Li-Ion batteries charged at voltages below 4.2?
2: In 9.3.2.1 in the datasheet of BQ77915 I read "In the event of an overvoltage fault condition on a particular cell, the balancing FET corresponding to that cell is turned on until the cell voltage drops to the full charge voltage or until the cell has recovered from overvoltage fault condition, whichever occurs earlier". So in case of an OV does the CHG fet turn off or the balancing of that specific cell starts?
I'm trying to get maximum capacity from the battery, so I want it fully charged. I would choose BQ7791501 for extra 50mV in the OV treshold but OTC is higher than the temperature allowed for charging for Li-Ion batteries (45 degrees C).
Thanks in advance
Dmitriy
www.rmftek.com