Hello,
I test a BQ35100 with a 2S1P LLSH14. I have a sequence with 5h of relaxation then for 1h, I alternate between 200mA for 3s then 50mA for 1s. I see that the SOH discrease of 5% while I have a sequence but the capacity corresponds to 2.1% of the nominal capacity. The gauge is always active (GE in the GND).
I join the gg.csv and the file of the sequence.
Best regards
MicouSERCEL_2S2PLsh20.gg.csvPVS_2_2 decharge 25deg 2S1P LSH14.csv