Hello team,
The COMP pin is the output of the internal error amplifier.
An external compensation network comprised of resister R5, ceramic capacitors C5 and C8 is connected to the COMP pin.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team,
The COMP pin is the output of the internal error amplifier.
An external compensation network comprised of resister R5, ceramic capacitors C5 and C8 is connected to the COMP pin.
Dear Sir,
Please check the answer in this FAQ:
Dear Sir,
I found you reject the original answer.
Actually you can also found the formula of R5, C5 and C8 on datasheet page 17 and 18. It is very clear.
Do you have any other request?
Hi Helen,
Thank you for the answer.
Dear Sir,
For the boost converter, fc is customer defined, if there's no big load change in the system, therefore the load dynamic performance is not an issue, generally we set fc=5k Hz. But if there's some load dynamic requirement, generally, we set fc=10k-15k. higher fc is not recommended because of the right half plane zero limit.
You can check the GEA from the EC table. It is 190uA/V.