This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2575: Review circuit

Part Number: LM2575


Dear Ti and all.

I attach circuit a file below this.

 - current consumption

+18V: 100mA

+5V : 100mA

+3.3V : 150mA

Please, Review that circuit. 

Best Regards,

Inho Jeon.