This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Battery Calibration / MaxError

Normal 0 false false false EN-US X-NONE X-NONE MicrosoftInternetExplorer4 Hi,

I am using a smart battery pack which uses the bq20Z95 impedance track fuel guage. I have a question regarding recalibrating the MaxError. I am aware that Max error is incremented internally by 0.05% for every increment of CylceCount after the last QMAX update. My question is, how do I recalibrate the pack, once Max Error increases to 10%, to bring the Max Error down to 1%? I assume that there may be one or more cycle profiles that I can follow. Any guidance that you can provide will be helpful.

Thank you,

Ralph