This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5069: In-Rush Current Limit

Part Number: LM5069

Dear TI,

As far as  I understand from the datasheet, the adjustable current limit value is the same with in-rush current limit. These two values are not different. That is, if I set the current limit to 10A, then the in-rush current limit control will be 10A? Is that the case?

Best regards,

Ramazan Yaman