Other Parts Discussed in Thread: BQ25616
Dear Sir,
I need to develop a portable device powered by a LiPo single cell battery. The system need to charge battery with the correct current depending by the power supply used (5V and 500mA, 1A, 2A depending by the adapters). When the adapter is disconneted, the battery needs to supply the system only if the switch is on, otherwise the current consumpion must be 0A. When the adapter is connected the system must be powered by Vbus indipendently if the switch is on or off.
Now my questions:
I thought to use the BQ25606 as battery charger.
1. I read in the forum that it can recognize the adapter by USB sygnals, but if the USB is used by the host it's needed a USB switch. It's correct?
2. The battery charger can supply a regulater output voltage by SW or PMID. What is the right way to provide the power supply to the system, by using SW or PMID?
3. Whe the USB is not connected and the power switch is OFF (System non connected) what is the current asorbed by the BQ25606?
4. The scheme I thought is correct or there is a best way to connect the part I need?
Thank you.
Best Regards.
Giuseppe