Other Parts Discussed in Thread: BQ27Z561-R1, BQ25601D, , BQ27Z561EVM-011, BQSTUDIO
Hi Team,
I'm planning to use the BQ25601D charger together the BQ27Z561-R1 (or R2) device, so for this purpose, before made the production PCB's I'm thinking to use the following evaluation boards:
- BQ25601DEVM-877
- BQ27Z561EVM-011
connections of the charger board to the gauge board is not a trouble as clearly show inside the bq27z561EVM-011 EVM User's Guide (SLUUBU0–June 2018) figure 9 at page 13/19. The question if is possible use the BQStudio in same time, for ither boards. In other world if is possible to have two different istances of the BQStudio applications one related the BQ25601DEVM-877 charger board and one for the BQ27Z561EVM-011 gauge board active at the same time to check and monitor the two device at same time.
From the BQStudio video introduction (LINK) I can read:
"The idea is a single suite of tools that's extensible and flexible, and supports the full product line-- supports the full ecosystem, in a way. So if you're using multiple products we can deal with that gracefully in a single application. Its function is to help you evaluate battery management solutions products, to implement them in your system, to program them, calibrate-- you know, configure chemistry and so on-- set it up for your platform requirements, and then validate the configuration and make sure things are working the way that you like."
then is possible manage multiple board by using a single application, but is not clear if is possible to use BQStudio multiple istances with different boards at same time.
Best regards.
F.