hello,
I have two questions for you.
1.After Charge Safety Timer Expiration, do I have to read the register twice as shown below to make it a "No safety timer fault" in order to recharge?
To read the current fault status, the host has to read REG0C two times consecutively.
The 1st read reports the pre-existing fault register status and the 2nd read reports the current fault register status.
2.Can it be recharged even if the default mode is set to Charge Safety Timer Expiration?
best regards