This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55165-Q1: How to make device startup with 5V input?

Part Number: TPS55165-Q1

Hi,

This device, TPS55165-Q1 confused me. The device claims can work with 4V to 36V input (@ 12Vout), however my customer found our EVM cannot startup at 5V input. I checked the datasheet there is another spec: Vin-startup. The device needs a higher than 5.3Vin to make the device working. Is my understanding correct?

If so, it will be difficult for my customer to use it in their system. They require the system to startup with 5.0V input. Is there any workaround to make the device startup at 5.0Vin?

Thank you!

John